We detected that you are using an outdated version of Internet Explorer. The Sensi Wire Picker Tool no longer supports Internet Explorer version 8 and below to give you better experience while you search our Products and Cross Reference through modern browsers.
We recommend upgrading your Internet Explorer to at least version 9, or use an alternative browser such as Google Chrome or FireFox.
You may also browse our Product pages through this link.
Will it work for me?
Sensi thermostats are designed to work on most heating and cooling systems
Check your wires
First, you will need to remove the thermostat faceplate from the subbase. It should easily snap off to reveal the wires and terminal labels. If you see two sets of terminal labels, enter only the labels that correspond to your system type (Heat Pump or Conventional) as they are indicated in the Wire Picker.
Verify Compatibility
Conventional systems include boiler, gas furnace, radiant heat, electric heat and air conditioning. Heat pump systems include heat pump, dual fuel, geothermal
Sensi thermostat is not compatible with line voltage systems. A line voltage thermostat will typically have wires larger than 18 gauge and may not have terminal labels. If you’re unsure of your system voltage, you or a contractor should measure voltage using a multimeter. Sensi thermostat is rated for 20-30 VAC.
Sensi thermostats are not compatible with millivolt system. A millivolt (mV) system operates on very low power, less than one volt. Sensi is designed for 20-30 VAC systems.
If your old thermostat has wires attached to the following sets of terminals, the Sensi thermostat is not compatible with your proprietary or communicating system:
Your system is compatible but may need a common wire.
Based on your thermostat wiring, Sensi Wi-Fi Thermostat is compatible with no modifications. Your system will need a common wire to be compatible with Sensi Touch Wi-Fi Thermostat. Learn more about adding a common wire.
Our current Sensi thermostats will not work with your system. We are working hard to include your type of system in future thermostat models.
Hmm, something isn't quite right.
Let's go back and make sure that you've entered all the connected wires. There should be an R, RH, or RC wire attached to your thermostat.
Your system is compatible but needs a common wire.
Based on your thermostat wiring, your system will need a common wire to be compatible with Sensi Wi-Fi Thermostat and Sensi Touch Wi-Fi Thermostat. Learn more about adding a common wire.
We may need to take a closer look to see if your system is compatible. You can:
1) Take a picture of your wiring after removing the thermostat cover.
2) Contact our support team by email or phone.
Your system is compatible with most models but may need a common wire.
Based on your thermostat wiring, your system will need a common wire to be compatible with Sensi Wi-Fi Thermostat and Sensi Touch Wi-Fi Thermostat. Learn more about adding a common wire. If you are installing and plan to use the humidification and/or dehumidifcation feature, then your system is not compatible with models UP500W or 1F86U-42WF.
Your system may be compatible but has an accessory that is not.
Based off of your thermostat wiring, your system may be compatible but you have an accessory that is not yet compatible with Sensi. Please email our support team with a picture of your current thermostat wiring for further information.
This website uses cookies so that we can provide you with the best user experience and to deliver advertising messages and offers on the website that are relevant to you. To read more about the cookies we use and to change your settings see our Privacy Notice.